Skip to main content

Leon's restaurant

London, UK

bg-image

When installing an air conditioning system, most clients need to account for a considerable amount of outdoor space to accommodate a bulky condenser unit. But finding the right amount of space is a difficult task for stores or businesses in built-up areas.

A lack of space was also the issue restaurant chain Leon's had to overcome to find the right air conditioning system for its new Fenchurch Street restaurant. Based in London's West End, the restaurant needed to find the right system to deliver comfort and energy efficiency in a space-saving design.

"To install such a discreet and highly efficient air conditioning system will hugely benefit many high street retailers across the UK, but particularly in London, where sourcing outside space for a condenser can be challenging."

- Gary Piper, Synecore HVAC Manager

Keep looking, you'll never find me

Synecore, a trusted installation partner in the project, selected our VRV i-series as the best choice for the new property. An outdoor system installed entirely indoors with only grilles visible from the outside, VRV IV i-series is a total climate control solution for buildings that are tight on space.

For this project, Synecore chose to install two 5 HP VRV IV i-series: one for the restaurant area and another for the kitchen. Because the heat exchanger and compressor are separate, installing the system was a simple and cost-effective process, and avoided additional renovation projects such as a rooftop installation, sound insulation or adding more pipework.

Separating the heat exchanger and compressor also meant the system is very discreet and easily blends into the property's existing framework.

VRV IV

Revolutionising air conditioning

bg-image

The results of this VRV IV i-series installation did not disappoint. Aesthetically pleasing, practical, energy- efficient and easy to install, VRV IV i-series is the full package, and allowed Leon's to open its new restaurant sooner than expected. The installation also showed how our VRV IV i-series is a great solution for other high street retailers in Europe that need a climate solution with a space-saving design.

Learn more

Our other cases

  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • C&A

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • Claerhout Office

    Advertising agency Claerhout Communication House opted for our VRV IV total solution for their new open landscape office building which provides office space for 45 employees and a conference room for 150 guests.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • Immogra

    Daikin’s VRV IV system delivers modern aesthetics with invisible integration of HVAC.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • Prezzemolo Vitale - Palermo

    For the new Prezzemolo Vitale store in the historical centre of Palermo, a system was installed consisting of Daikin Zeas and VRV units.
  • Radisson Blu and Proximus

    The new Radisson Blue hotel in Bruges is located near Bruges station, an area which has seen extensive redevelopment over the past few years. Built by Belgian property developer Group GL, the impressive new tower complex houses not only the new hotel but also a 6,000 square metre area of office space, currently occupied by GL tenant Proximus.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Biocoop

    Daikin completes the installation and commissioning of the first transcritical CO2 refrigeration solution on the French market at a meat processing laboratory in the Dordogne.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Ibis Budget Hotel, Ghent

    In March 2018, the new IBIS budget hotel opened its doors at the Dampoort in Ghent, offering guests outstanding comfort in a modern attractive setting. For the building owner Viktor De Maertelaere, investment in an energy efficient and reliable climate control system was key to the budget hotel concept.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.
  • Sound enclosure case study in Flassy

    The acoustic effectiveness of Daikin’s new Sound Enclosure for its Sky Air and VRV 5 outdoor units has been validated by field trials undertaken at a residential installation in Burgundy, France, showing significant sound reductions equal to and even exceeding factory test room values.
  • Supplying a temperature control solution for a railway control system

    Daikin has recently supplied a total solution to maintain temperature in the train switching system control room of a French intercity high-speed rail service.
  • VRV 5 decarbonises Lincoln University

    The University of Lincoln is setting new standards in sustainable building management with the installation of a new R32-based VRV5 Heat Recovery heat pump, underlining the university’s commitment to environmental improvement and a significant move towards its net zero targets.
  • Las Arenas

    When it came to upgrading existing VRV systems to reduce maintenance costs and further improve comfort control, choosing a replacement solution with lower CO2 footprint was top of the agenda.
  • Supplying a complete HVAC system for an office building

    Daikin has recently supplied a complete solution for an office building of a Dutch company in the flower import/export business.
  • Providing a cooling solution for an office building in the UAE

    Daikin recently supplied four chillers for the Headquarters of the Emirates police force, in the UAE. The chillers will be used to provide cooling through air handling units through the large building and ensure the maximum level of comfort for occupants.
  • Supplying a hospital with an efficient, reliable, and compact solution

    Daikin recently supplied a chiller for a big hospital in Oman. The hospital’s capacity was extended with the opening of a new wing, which required the HVAC system to be integrated with a new chiller to meet the greater cooling needs of the building. For this project, it was essential to find a reliable solution with advanced technology that could perfectly meet the needs of the facility.
  • Providing cooling for the High-Luminosity LHC project at CERN

    Daikin recently supplied 8 water-cooled chiller units to CERN to provide cooling for the High-Luminosity LHC (Large Hadron Collider) project. The High-Luminosity LHC project aims to boost the performance of the LHC to increase the potential for discoveries after 2029. The goal of the project is to increase the integrated luminosity by a factor of 10 beyond the LHC’s design value. That will allow the gathering of a higher quantity of data and observations of rare processes as the increase in luminosity will make the LHC more powerful.
  • Caleido Tower, Madrid

    The Caleido Tower, also known as the Fifth Tower, is situated in the business district of Paseo de la Castellana in Madrid.