Skip to main content

The streamer technology developed by Daikin Industries is an epoch-making air purification technology that has succeeded in stably generating "high-speed electrons", which has been difficult until now.

Harmful proteins and chemicals exist around us

Such as smoke, pollen, allergies, bacteria, etc...

About streamer discharge

The streamer discharge, a type of plasma discharge, to generate a high oxidative decomposition force "fast electrons" three-dimensional-extensive,
as compared to conventional plasma discharge (glow discharge), oxidative decomposition force 1,000 times That's it.

In this technology, high-speed electrons combined with air components have a strong oxidative decomposition power, so
they continuously act on odors, fungi, and formaldehyde, which is a indoor pollutant.

It has been demonstrated in collaboration with universities and public research institutes
to act on harmful substances such as attenuated influenza virus and norovirus, toxins and bacteria that cause food poisoning