Skip to main content

Air-to-air heat pumps

Cool and heat your space using renewable energy.

Get year-round comfort in your shop, B&B, restaurant, home office or any other commercial building with advanced, efficient heating and cooling technology. Air-to-air heat pumps transfer heat between the outdoor air and the building using refrigerant gas. By adding a tank, you can also have domestic hot water. 

Energy efficiency reduces bills and emissions

Enjoy comfortable temperatures whatever the weather

Improve the air quality in your commercial space

Elegant design fits your interior

Designed to suit your taste

Our air-to-air heat pumps can be configured in different ways, that work for your space. You can add indoor units to up to 5 rooms. 

bg-image

Find the perfect solution

What type of solution are you looking for?

More information

The air-to-air heat pump indoor unit is the part of an air-to-air heat pump system that’s located within the home, and provides the conditioned air into the space.

The choice of an air-to-air heat pump indoor unit depends on your specific needs but it's important to understand how the system works as a whole. There are different air-to-air heat pump systems (also known as air conditioners), each with its own unique characteristics. One of the most popular types used in homes is a split system, which is split into two units: one indoors and one outdoors. While heating, the outdoor unit extracts heat from the outside air and transfers it inside via the indoor unit, or reverse when cooling your home.


There are three types of air-to-air heat pump indoor units:

Wall-mounted units

Wall-mounted models (Stylish, Ururu Sarara, Daikin Emura, Perfera,) come in different sizes and colours to match with your interior.

Floor-standing units

Floor-standing models (Perfera Floor) are compact air conditioner that fit perfectly under a window sill or in a room where the height is limited.

Concealed ceiling units

Concealed ceiling units. If you don't want a visible indoor unit, a concealed air-to-air heat pump can be installed in suspended ceilings or false walls.

An air-to-air heat pump (also known as an air conditioner) is typically composed of two units: The indoor and outdoor unit. These are usually called ‘split’ systems.

The split outdoor unit, mounted on an exterior wall or positioned in a garden or on a roof, is the part of an air-to-air heat pump that contains the compressor, propeller fan, circuit board and heat exchanger. The outdoor unit compresses the refrigerant that extracts or emits heat or cold in the room to or from its companion indoor unit.

Yes, and if you renovate your property and switch to a renewable air conditioner, you will add value to your renovated commercial building, the environment, and your bottom line. Heat pumps can be installed in almost any commercial building. However, there are some considerations that may need to be addressed, particularly regarding insulation. For a heat pump to function efficiently, your building needs to be well-insulated to prevent as much heat from escaping as possible. A suitably qualified heating engineer can advise you on what needs to be done in your building to make it suitable for a heat pump system. This might include upgrading the insulation of your walls and roof. You also need to consider the location. The outdoor unit will need to be installed outside your building and should be in a place that you can access easily when you need to clean the unit, adjust its settings, or have the heat pump serviced.

Yes, an air-to-air heat pump (also known as an air conditioner) can bring hot water to your commercial building. With Daikin's Multi+ solution, heating, cooling and hot water are supplied with one system. It connects up to three units and one domestic hot water tank and is compatible with a 90 and 120-litre tank and a wide range of indoor units, offering unrivalled flexibility. Our Multi+ solution includes an intuitive full-text display on the domestic hot water tank for monitoring and adjustment of all settings, including scheduling and water temperature.

Daikin's air conditioner can give you relief from your allergies because they can capture the allergens in the air conditioner filter and improve the quality of air that you are breathing. Not only do our air conditioners keep you warm and cool but they are also removing pollutants, pollen and particle matter from your breathing space.

Some Daikin units are also equipped with a Flash Streamer and different filters like the titanium apatite deodorising filter or the silver allergen removal filter, which are able to reduce the pollutants in the air quickly and efficiently.

No! Furthermore, our air conditioners (also known as air-to-air heat pumps) can help reduce the symptoms of allergies. Daikin integrates multiple filters in all its air conditioning units: titanium deodorising filters, silver allergen filters and flash streamers remove dust and capture bacteria. With proper air conditioning maintenance, and as long as they are cleaned regularly, these filters will provide cleaner, healthier air for everyone to breathe.

For your heat pump to function as it should, it is essential that the system is installed correctly. Only an authorised technician should carry out the installation and in a suitable location. The surface must be firm enough to withstand the weight and vibrations of the unit and there must also be sufficient space for airflow and for connecting pipes and power cables. Any plants or shrubs that may be located near your heat pump should be at least a metre away and regularly pruned. The pump should also be installed in a place that’s easy to access for services and other general maintenance.

We often get asked why we can’t put the heat pump inside. Could they not be placed in the loft or conservatory? The answer to this is no. This is because, after a few hours, the heat pump will have extracted all of the warmth from the trapped air, effectively turning this space into a freezer. This is why air-to-air heat pumps need access to the free-flowing outside air.

We advise having a service done by a qualified engineer once a year. Scheduled servicing, regular maintenance spot-checks and routine cleaning of the system will extend its lifespan and maintain its energy efficiency.  

Here are some signs your air conditioner needs immediate maintenance:

If your air conditioner unit makes more noise than usual, the filters may be clogged. Clean the unit by removing dust with a vacuum cleaner. If the same noise persists or you hear a gurgling sound, there could be a mechanical issue. A qualified technician should then be called to examine the unit.

New built

When building a new building with high insulation, a Daikin air-to-air heat pump fits all heating and cooling needs. Plus, their A+++ energy efficiency ratings and low environmental impact meet all green building requirements.

 

Replacement of electric heating

 

An air-to-air heat pump is the ideal solution when replacing electric heating.
Our flexible units are easy to install, offering several designs to fit your needs the best. With up to A+++ energy efficiency ratings both in heating and cooling, you can save a lot on your energy consumption.


NEW: Multi+ is an all-in-one system to offer heating, cooling and domestic hot water for houses up to 80m².

Quickly reduce your energy consumption

If your current heating system is not yet outdated, but you want to reduce your energy consumption, you could consider installing an air-to-air heat pump as add-on system. This will give you the opportunity to use your heat pump for heating and cooling and only use your current heating system for hot water production.

Best-in-class energy efficiency

Daikin air-to-air heat pumps offer up to A+++ energy efficiency thanks to a number of advanced solutions. Our signature inverter technology, for example, reduces the energy consumption by up to 30% compared to a non-inverter system, simply by adjusting the speed of the motor as required instead of shutting it down and starting it back up completely.

 

equipped with our signature inverter technology
Illustration of five connected Daikin Units

Cool and heat up to 5 rooms

Daikin air-to-air heat pumps offer a range of options: either connect a single indoor unit to one outdoor unit, or use our multi-split system to connect up to five indoor units to one outdoor unit. The multi-split system allows you to efficiently cool or heat up to five different rooms to different temperatures.

Learn more

Only one system for hot water and air conditioning

Our new Multi + range connects a single outdoor unit with up to 3 indoor units and a domestic hot water tank of 90 or 120 litres. Domestic hot water, cooling and heating is the key strength of this affordable all-in-one system.


Learn more

Illustration of five connected Daikin Units