Skip to main content

In which Refrigeration systems can I use Electronic expansion valves?

Pulsating electronic expansion valves can be used on following systems:

Refrigeration systemSingle EvaporatorMultiple Evaporators
Conveni PackNoYes
Single Zeas unitNoYes
Multi Zeas unitsNoYes
Booster unit (with Zeas or Conveni Pack)NoYes

 

Proportional electronic expansion valves can be used on following systems:

Refrigeration systemSingle EvaporatorMultiple Evaporators
Conveni PackYes, with condition*Yes
Single Zeas unitYes, with condition*Yes
Multi Zeas unitsYes, with condition*Yes
Booster unit (with Zeas or Conveni Pack)Yes, with condition*Yes

* For Single Evaporator systems, Proportional type of expansion valves are allowed if the time between fully open to fully closed is less than 5 s!

Need help?

Find more information

Need help?

Find more information

Need help?

Need help?

Need help?

Looking for a new challenge?