Skip to main content

Which Evaporator Pressure Regulators (EPRs) can be used with R410A?

The EPRs used for refrigeration must meet the following conditions.

  1. PS ≥ 25 bar
  2. No bypass is required for oil recovering
  3. EPR can be used when connecting to 100% of the refrigerators/evaporators like for example to protect the goods from the winter function
  4. Minimum capacity ratio of 50%
  5. When using an EPR the total load of the system must always be minimum 2 kW
  6. There are no limitations on the number of EPRs used

When several ZEAS units are used in a project, please group all the refrigerators or evaporators with the same requested evaporation temperature to the same Zeas unit. This to optimize the efficiency of the refrigeration system.

Need help?

Find more information

Need help?

Find more information

Need help?

Need help?

Need help?

Looking for a new challenge?