Skip to main content

What is sound pressure/sound power?

Sound pressure level (Lp)  

Is a measure of the sound energy emitted from a source of noise, expresses in decibel or dBA

Sound power level (Lw)  

Is the above but measured in predefined conditions  
The sound power level is independant on:

  • the location of the equipment
  • the environmental conditions, and 
  • the distance from the measurement point

The sound power level can be considered as the more precise of the two. The sound power will have a higher value than the sound pressure, bon't be mislead by this. 

The impact of decibels:

Lp dB(A) Perceived loudness Sound 
0Treshold of hearing-
20Extremely softRustling leaves, quiet room
40Very softRefrigerator humming
60Moderately loudNormal conversation, restaurant
80Very loudCity traffic, lorry
100Extemely loudSymphonic orchestra, farm tractor
120Treshold of feelingJet taking off

Need help?

Find more information

Need help?

Find more information

Need help?

Need help?

Need help?

Looking for a new challenge?