Skip to main content

I do not succeed in connecting the adapter to the wireless network by using the “WLAN settings” menu.

Try the following:

  • Follow the setup guide in the application1
  • If the setup guide does not solve the problem:
  1. If your network is not visible, refer to “My network is not visible in the network dropdown list”.
  2. Make sure your wireless network name (SSID) does not include special characters such as “ ‘, %, &, ?, +, =, …” or non-ASCII characters. They are not supported by the WLAN adapter.
  3. Make sure to use a compatible security setting. The WLAN adapter supports only WPA or WPA2 personal encryption. WEP encryption is not supported.

 

The setup guide (“Add adapter”) can be accessed through the main menu.

FAQ onlinecontroller direct-connection to the adapter ap mode the adapter is not visible

Need help?

Find more information

Need help?

Find more information

Need help?

Need help?

Need help?

Looking for a new challenge?