Skip to main content

How can I re-initialize the WLAN adapter to the factory default settings?

Caution: factory resetting the WLAN adapter also clears all settings. You will need to setup the WLAN adapter again to match your preferences.

Settings that are reset:

  • Home network connection (WLAN settings)
  • Out-of-home account information
  • Child lock code
  • Schedule timers (including schedule function of demand control1)
  • Energy consumption data1
  • Unit name and icon

You can factory reset the adapter with following instructions:

On the WLAN adapter:

  1. Press both “Setup” and “Mode” buttons simultaneously till all LEDs are blinking.
  2. Release both buttons.
  3. Press the “Setup” button shortly: all LEDs will start to blink quickly.
  4. Wait till the “Power” LED is continuously lit. The adapter has been reset successfully. 

Only if the unit supports this function

Need help?

Find more information

Need help?

Find more information

Need help?

Need help?

Need help?

Looking for a new challenge?